Skip to main content
spa23
Associate III
Jun 7, 2017 7:11 AM UTC
Solved

X-NUCLEO.IDW04A stuck in reset

Posted on June 07, 2017 at 09:11

HI 

We are planing to use a new WIFI module from ST for replacing the old module ( form another supplier )  

so I :

1. bought a NUCLEO-F401RE and a X-NUCLEO.IDW04A boards.

2. downloaded the en.x-cube-wifi1_firmware software. 

3. done the board setup according to page 6 in UM2183 (Getting started with the X-NUCLEO-IDW04A1)

4. compiled the firmware (Server_Socket) with IAR, and downloaded it to the board.

5. run.

and now the software get stuck in the wifi_reset() function wating for the stage to get started.

while(IO_status_flag.WiFi_WIND_State != WiFiHWStarted)

{

__NOP(); //nothing to do

} 

so before I get started with the big investigation, I was thinking that maybe I wasn't the only one that have see this problem.

So I'm hoping that one of you guys can give me a hint, thanks in advance..

#x-cube-wifi1 #spwf04sa #x-nucleo-idw04a1
    This topic has been closed for replies.
    spa23
    spa23Best answer
    Associate III
    Jun 7, 2017 1:06 PM UTC
    Posted on June 07, 2017 at 15:06

    Thanks, I found a solution:

    - to use SW Reset functionality (wifi_reset() function)

        - jumper on position JP3 (middle and top) is required (was not mounted) 

    3 replies

    Mridupawan Das
    Visitor II
    Jun 7, 2017 12:02 PM UTC
    Posted on June 07, 2017 at 14:02

    Hi,

    By default, the build is set for SPWF04 and SPI interface. So if you are using UART as interface please set the required macros in the file wifi_conf.h in the Inc folder of the App you are running (e.g. server socket in your case).

    Also check out the correct jumper settings for UART/SPI for the SPWF04 in the readme files.

    IN case of UART it should be as below for the F401 board (not the comment out for SPWF01):

    #ifdef USE_STM32F4XX_NUCLEO 

    #define CONSOLE_UART_ENABLED

    //#define SPWF01

    #define SPWF04

    regards,

    Mridu

    Mridupawan Das
    Visitor II
    Jun 7, 2017 12:04 PM UTC
    Posted on June 07, 2017 at 14:04

    you can also go through other threads discussing different versions of issues:

    https://community.st.com/0D50X00009XkXvmSAF

    https://community.st.com/0D50X00009XkgFFSAZ

    spa23
    spa23AuthorBest answer
    Associate III
    Jun 7, 2017 1:06 PM UTC
    Posted on June 07, 2017 at 15:06

    Thanks, I found a solution:

    - to use SW Reset functionality (wifi_reset() function)

        - jumper on position JP3 (middle and top) is required (was not mounted)