Skip to main content
BSalt.1
Associate III
Apr 4, 2022 9:28 AM UTC
Question

X-Nucleo-IDB05A1 boards problem

I have a few X-Nucleo-IDB05A1 boards, and when I test them on the X-Cube64 board, some work and some don't. So I checked it, and like the attached picture file, the Trace Code and Bulk ID are different.

Trace code XN915011 is fine,

11540270 doesn't work at all.

What's the matter?

0693W00000LwlX7QAJ.jpg0693W00000LwlXbQAJ.jpg

This topic has been closed for replies.

2 replies

Sebastien DENOUAL
ST Employee
Apr 7, 2022 12:50 PM UTC

HI @BSalt.1​ ,

Do you confirm Jumper and solder bridges configuration are exactly similar on both boards ?

Thanks,

Sebastien.

BSalt.1
BSalt.1Author
Associate III
Apr 11, 2022 4:46 AM UTC

@Sebastien DENOUAL​ 

Hi,

Yes the idb05A1 board has only one 2pin jumper block and some 0 ohm jumpers that need to be replaced by soldering, both types of boards are factory-set.

Thanks,

Ewing.