Skip to main content
andreaspiezia9
Associate III
Sep 2, 2019 8:42 AM UTC
Question

X-NUCLEO-IDB05A1 and NUCLEO_F401RE not working with X-CUBE-BLE1

Hi,

I'm starting to play around with ST BLE.

I'm using X-NUCLEO-IDB05A1 on NUCLEO-F401RE.

I've just followed the "Getting started" https://www.youtube.com/watch?v=AIJA4yRxuP4

  1. I've drag .bin over the icon: NUCLEO_F401RE (C:\Users\andre\Documents\BlueNRG MS Stack\en.X-CUBE-BLE1\en.X-CUBE-BLE1\STM32CubeExpansion_BLE1_V4.4.0\Projects\STM32F401RE-Nucleo\Applications\SensorDemo\Binary)
  2. Board is fleshed and LD2 is green

But BlueNRG App v1.1 doesn't recognize any device.

What could I check to find the problem?

Thanks a lot

This topic has been closed for replies.

4 replies

alok
Visitor II
Sep 8, 2019 1:20 AM UTC

Hi,

Do you have other boards to verify the behavior ?

Can you check in debugging if the BLE is getting initialized or not.

Can you check in the BLE scanner or any application if the board is recognized or not

Thanks

andreaspiezia9
Associate III
Sep 10, 2019 3:59 PM UTC

Hi Alok,

I've commented the UART init (probably only used for PRINTF?) and I went ahead and found a problem in MX_BlueNRG_MS_Init -> getBlueNRGVersion -> staus of hci_le_read_local_version(...) return an ERROR (0xFF).

Do you have an idea? Do you have working code as example?

Thanks a lot

uint8_t getBlueNRGVersion(uint8_t *hwVersion, uint16_t *fwVersion)
{
 uint8_t status;
 uint8_t hci_version, lmp_pal_version;
 uint16_t hci_revision, manufacturer_name, lmp_pal_subversion;
 
 status = hci_le_read_local_version(&hci_version, &hci_revision, &lmp_pal_version, 
				 &manufacturer_name, &lmp_pal_subversion);
 
 if (status == BLE_STATUS_SUCCESS) {
 *hwVersion = hci_revision >> 8;
 *fwVersion = (hci_revision & 0xFF) << 8; // Major Version Number
 *fwVersion |= ((lmp_pal_subversion >> 4) & 0xF) << 4; // Minor Version Number
 *fwVersion |= lmp_pal_subversion & 0xF; // Patch Version Number
 }
 return status;
}

andreaspiezia9
Associate III
Sep 8, 2019 6:15 PM UTC

Hi Alok,

thanks a lot for your reply.

Board works good with others projects.

I'm debugging the code mode in deep and find a problem in the MX_USART2_UART_Init, it return BSP_ERROR_PERIPH_FAILURE.

It has called by MX_BlueNRG_MS_Init(void) -> User_Init(void) -> BSP_COM_Init(COM1).

Do you have suggestions?

int32_t BSP_COM_Init(COM_TypeDef COM) 
{
 int32_t ret = BSP_ERROR_NONE;
 
 if(COM > COMn)
 {
 ret = BSP_ERROR_WRONG_PARAM;
 }
 else
 { 
 hcom_uart[COM].Instance = COM_USART[COM];
#if (USE_HAL_UART_REGISTER_CALLBACKS == 0)
 /* Init the UART Msp */
 USART2_MspInit(&hcom_uart[COM]);
#else
 if(IsUsart2MspCbValid == 0U)
 {
 if(BSP_COM_RegisterDefaultMspCallbacks(COM) != BSP_ERROR_NONE)
 {
 return BSP_ERROR_MSP_FAILURE;
 }
 }
#endif
 
 if (MX_USART2_UART_Init(&hcom_uart[COM]))
 {
 ret = BSP_ERROR_PERIPH_FAILURE;
 }
 }
 
 return ret;
}

ASPIE.5
Associate II
Sep 9, 2019 12:40 PM UTC

What UART is used for in that application?