Skip to main content
ivan239955_st
Associate
Jul 25, 2016 5:57 AM UTC
Question

X-Nucleo-IDB04A1 interface STM32F217

Posted on July 25, 2016 at 07:57

Hi,

I want to interface X-Nucleo-IDB04A1 (BlueNRG) with STM32F217 (using STM3221G Eval board). I have used the SensorDemo in X-cube-ble1 (for X-Nucleo-IDB04A1 and Nucleo-L053R8 ) and I have re-adpated the files to be compatible with STM3221G Eval board, that is the port mapping and all drivers, I run the code and i find no errors. I load the application and I get nothing when testing with my Android phone 4.4 (BLE compliant). 

Could anybody give me some tips on how I can work this around? Thanks

Steps I have taken into this approach:

1- Connect the pins to Corresponding SPI pins

2- Include all drivers for the STM32F217 to be recognized by the compiler

3-add lines to USE the STM322xG_Eval in all relevant files (C and h)

4-Check relevant include paths, and files

5- Build all target (no errors) and load

#stm32f217 #x-nucleo-idb04a1
This topic has been closed for replies.