X-NUCLEO-67W61M1 getting stuck during initialisation
- 2 replies
- 946 views
Title edited with correct board part number.
Hello ST Community,
I’m working on integrating the NUCLEO-W67W62M1 Wi-Fi module with an STM32H723ZG(spi ptotocol) board using the Arduino connectors.
I followed the official documentation for the CLI example and generated the .ioc project accordingly. The project builds and flashes successfully, but I’m getting stuck during the modem initialization.
-
Host MCU: STM32H723ZG (Nucleo-H723ZG board)
-
Wi-Fi Module: NUCLEO-67W61M1
-
Connection: Arduino connectors
-
Firmware on Wi-Fi module: t01.bin (flashed in standalone mode)
-
Example used: CLI project generated from STM32CubeMX (following ST documentation)
-
RTOS: FreeRTOS(cmsis-v2) (default configuration)
problem1:
During initialization in W61_AT_ModemInit(W61_Object_t *Obj), the function fails at the semaphore wait:
xReturned = xSemaphoreTake(mdm->sem_if_ready, pdMS_TO_TICKS(4000));
if (xReturned != pdPASS) { SYS_LOG_ERROR("sem_if_ready not received\n"); ret = -1; goto __err; }
problem 2: