Skip to main content
Maciej Wolejko
Visitor II
May 15, 2017 8:53 AM UTC
Question

www.st.com

Posted on May 15, 2017 at 10:53

Now I am working with SP1ML(STEVAL-SP1ML868) and SPSGRF(X-NUCLEO-IDS01A4) modules working on 868 MHz frequency. SP1ML(USB Dongle) is connected to my MacBook where I can see what 

SPSGRF is sending to me in 

Putty software. SP1ML had a 

standard firmware, allowing AT commands to facilitate RF configuration, data transmission and reception, using simple point-to-point communication.

SPSGRF was programmed

 using expansion software package

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-software/x-cube-subg1.html

. I have two problems with connection between my modules.

First of all SPSGRF is sending to me very weird strings shown below:0690X00000603qEQAQ.jpg 

Below I have posted one more images showing the configurations of SP1ML module and code from Keil showing a configurations of SPSGRF module 

https://codepaste.net/kxohms

. I checked: this is not problem with Baud Rate but I think it is problem with radio configuration. I also changed S28: PAYLOAD_SIZE to other value, but that didn't change anything.0690X00000606wGQAQ.png

The second one is that I cannot send any data from SP1ML to SPSGRF. 

Did anyone have a similiar problem?

Tann.

#wireless #spirit1 #spirit1-sp1ml #spsgrf #spi
This topic has been closed for replies.