Skip to main content
Gerardo GALLUCCI
ST Employee
Nov 30, 2017 10:16 AM UTC
Question

www.st.com

Posted on November 30, 2017 at 11:16

SPWF04Sx FW1.1.0 now online!

Dear community,

FW1.1.0 for SPWF04Sx series of Wi-Fi modules has been released! Please update your SPWF04Sx devices, so you can have the access to new features and fix for bugs and vulnerabilities. Link 

http://www.st.com/content/st_com/en/products/embedded-software/wireless-connectivity-software/stsw-wifi004.html

.

This is a list of new delivered features:
  • WPA2 security in miniAP mode
  • ECDH and ECDSA algorithms for TLS key exchange (ECC)
  • MicroPython classes for TFTP, HTTP, SMTP, MQTT and WebSocket clients
  • AT+S.FSM command for filesystem mount
  • ramdisk_memsize configuration variable to set the length of RAM_disk
  • 2 new GPIOs, 19 and 20, from module's bottom
  • another PWM instance
  • increased webserver capability, now able to support up to 4 parallel HTTP Post request
  • support for 8MB SPI flash from Macronix

Moreover, WPA2 vulnerability has been fixed. This is a list of others fixes:

  • garbage collector in microPython environment
  • SPI management, including chip select, frame header, and CrLf removal from asynchronous events
  • watchdog coming from AT+S.INPUTSSI command
  • mixing output_demo WIND:57 with others synchronous (AT-S.event) events
  • duplicated character at the end of MQTT WIND:86
  • memory leak in AT+S.FSP command
  • PWM reload

A few changes in backward compatibility have been introduced:

  • WIND:29 in miniAP now adds STA MAC address
  • PWM command now needs an ID, since a new instance has been added
  • give an higher priority to SDCard, rather than RAM disk, when no path is specified
  • SPI management of synchronous (AT-S.event) events now takes care of console_verbose configuration variable (set this variable to 0 to ensure fully compatibility with FW1.0.0)

Some bugs were found and raised also into this forum, so, thanks to you guys!

Last but not least, WIFI1 package FW3.1.0 for X-NUCLEO-IDW04A1 Wi-Fi shield has been released too. It adds MQTT, TFTP, Websocket and SMTP management. Link 

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-wifi1.html

.

For STM32+SPI users, please be sure to use FW3.1.0 of WIFI1 with FW1.1.0 of SPWF04.

#spwf04 #spwf04s #spwf04sx #spwf04sc #spwf04sa
    This topic has been closed for replies.

    1 reply

    kenneth er
    Associate
    Dec 6, 2017 11:02 AM UTC
    Posted on December 06, 2017 at 12:02

    Hi, 

    I was trying out the latest 

    WIFI1 package FW3.1.0 for X-NUCLEO-IDW04A1 mentioned in this post, and I think you missed out the definitions in the wifi_conf.h file. The previous version has definitions for different projects but this one is missing many definitions. Not sure if this is the intended design but definitely not helpful for someone learning to use the wifi module through the example project, since they can't just compile and run.