Skip to main content
dworkman
Associate
Mar 30, 2016 10:04 PM UTC
Question

WIND:11:Initial SPI read failed

Posted on March 31, 2016 at 00:04

I just fired up the SPWF01S module on a prototype board that I made. 

Got WIND:1, WIND:13, WIND:3, WIND:0, then this error over and over.

I didn't send anything to the module. 

Did I forget to connect something, is the module requiring setup, or is the module damaged?

Thanks

#initial-spi-read-failed
    This topic has been closed for replies.

    3 replies

    Gerardo GALLUCCI
    ST Employee
    Mar 31, 2016 6:11 AM UTC
    Posted on March 31, 2016 at 08:11

    Hi David,

    a timeout value was increased inside current FW3.5. That error should not be observed anymore (if module is sane...)

    Which FW version are you using?

    BR

    j

    dworkman
    dworkmanAuthor
    Associate
    Mar 31, 2016 1:19 PM UTC
    Posted on March 31, 2016 at 15:19

    I get this at powerup:

    WIND:1:Poweron (141106-0950875-SPWF01S)

    Which number in there is FW version?

    Gerardo GALLUCCI
    ST Employee
    Mar 31, 2016 1:24 PM UTC
    Posted on March 31, 2016 at 15:24

    It's FW3.3.

    November 2014