Skip to main content
MK..1
Associate III
Feb 11, 2026 10:29 PM UTC
Question

wiFi Fine Timing Measurement (FTM) IEEE 802.11mc WIFI

Hi

Does ST have any WIFI chip with FTM?

Thanks

11 replies

Peter BENSCH
ST Technical Moderator
Feb 14, 2026 8:42 PM UTC

No, ST does not offer Wi‑Fi FTM. But if you outline your use case, an alternative solution within the ST portfolio might be possible.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MK..1
MK..1Author
Associate III
Feb 16, 2026 4:35 PM UTC

Hi

what I need to do is to synchronise 2 devices over WIFI.

I need a 32 bit timer on stm32 which runs with less than 50 microsencond accuracy in comparison to a second device which also has a STM32.

One device may be configured as client and the other device as router or server.
Does the ST framework give me access to : (TSF) Timing Synchronization Function of 802.11?

See here:

https://en.wikipedia.org/wiki/Timing_synchronization_function

 

 

Andrew Neil
Super User
Mar 2, 2026 9:37 AM UTC

@MK..1 wrote:

less than 50 microsencond accuracy (sic?) in comparison to a second device


You mean less than 50 us error ?

 

But, as @Peter BENSCH said, you still haven't said why you (think you) need this ?

ie, what is your end goal here? What are you trying to achieve ?

 

Describe the goal, not the step.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MK..1
MK..1Author
Associate III
Mar 2, 2026 9:10 AM UTC

Hi  @Peter BENSCH 

any news here?

Do you know: Does the ST framework give me access to : (TSF) Timing Synchronization Function of 802.11?

Thx

MK..1
MK..1Author
Associate III
Mar 2, 2026 10:36 AM UTC

Hi @Andrew Neil 

thanks. 

On my STM32 device I want to make a ADC measurement. 

I don't have one device but 10 (or lets say n) devies. All these 10 (or n) embedded Devices are connected via WIFI. 

I want all these 10 devices to initiate the ADC conversion at the same time (+/- 50 us accuracy). 

For this purpose I want synchronise all devices with an accuracy of ~50 us. 

Did I manage to describe it properly? ;)

Andrew Neil
Super User
Mar 2, 2026 10:46 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MK..1
MK..1Author
Associate III
Mar 2, 2026 11:00 AM UTC

@Andrew Neil ideally i would stay withhin the STM32 world (ESP32 is not from ST?). Is this possible with ST's offerings as well? 

Second Question: Does the ST framework give me access to : (TSF) Timing Synchronization Function of 802.11?

Thx

Andrew Neil
Super User
Mar 2, 2026 11:06 AM UTC

@MK..1 wrote:

ESP32 is not from ST?


Correct.

 


@MK..1 wrote:

Second Question:


Best to keep to 1 question per thread - start a new thread for a separate question ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Mar 2, 2026 11:19 AM UTC

@MK..1 wrote:

Does ST have any WIFI chip ...


Currently, ST's only WiFi product is the ST67W611M1  module.

It supports IEEE 802.11b/g/n/ax:

https://www.st.com/en/wireless-connectivity/st67w611m1.html

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MK..1
MK..1Author
Associate III
Mar 2, 2026 11:42 AM UTC

By anay chance : do you know if ST67W611M1 provides access to (TSF) Timing Synchronization Function?

Andrew Neil
Super User
Mar 2, 2026 11:46 AM UTC

Again, that's a separate question.

But I don't know.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.