Skip to main content
Don david
Associate
Apr 11, 2017 10:12 AM UTC
Question

WIFI DIRECT MODE and 3G/4G connectivity

Posted on April 11, 2017 at 12:12

Hi All,

I need some suggestion regarding my project.

I want  my device to send data in wifi direct mode to the Android device which has 3g/4g connectivity.The Android device  will then forward the data to the server , so that live tracking happens.

Can Anybody tell how to proceed with this

Kind Regards

Don David

#android #wifi-direct
    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Apr 11, 2017 4:56 PM UTC
    Posted on April 11, 2017 at 18:56

    Hi David,

    ST SPWF0xS modules are not implementing WiFi Direct mode. You can setup the ad-hoc mode, called IBSS into datasheet and user manuals. Or, better, use the miniAP capability. You can setupSPWF module to act as a basic AP, providing link up to 5 devices. Also DHCP/DNS servers are running in this case!

    Please refer to this discussion:

    https://community.st.com/0D50X00009XkY8pSAF