Skip to main content
Scott Löhr
Senior III
Sep 14, 2018 11:31 PM UTC
Question

Why does BlueNRG-MS, v7.2c, wait forever after this call: aci_gap_create_connection(ScanInterval, ScanWindow, sType[sIdx], sAddr[sIdx], PUBLIC_ADDR, ConnInterval, ConnInterval, ConnLate, ConnTimeout, ConnLength, ConnLength);

After the call returns BLE_STATUS_SUCCESS, but the target BLE Peripheral slave device stops advertising forever (i.e. a race between scan result, connection request and peripheral stop advertising/go out of range)?

It would be nice if a connection request timed out in a similar way to how a general scan times out (with a GAP procedure complete, 0x02). Now I have to babysit the BlueNRG-MS with my own timer after making a connection request - is there an easier way?

Thanks,

    This topic has been closed for replies.

    2 replies

    nick239955_stm1_st
    Associate II
    Dec 20, 2018 10:07 PM UTC

    I have come across the same issue and agree with Scott that it would be nice if the connection request timed out rather than trying forever.

    RAdam.1
    Associate III
    Feb 8, 2021 6:07 PM UTC

    @nick239955_stm1_st​  and @Scott L�hr​  I agree - how did you end up terminating the attempted connection? Is there a function or a call back that will just make it stop and recover? I cant do a thing once it is waiting to connect!

    Any help would be greatly appreciated