Skip to main content
Anitha
Associate III
May 7, 2019 1:20 PM UTC
Question

While sending the data from the app to node which function call calls first to receive the sent data?

I'm sending some data from nRF Connect app to node I want too see that data in firmware debugging. Where can I see that data? I mean in which function call?

This topic has been closed for replies.

1 reply

alok
Visitor II
May 13, 2019 7:41 AM UTC

If you are using the BLE-Mesh firmware, please use corresponding "ST BLE Mesh" App from play store

If you are using the Generic model for LED on-off: The entry point is "GenericModelServer_ProcessMessageCb()"

For Vendor Model, the implementation is in Vendor.c. The entry point for message from App is "Vendor_WriteLocalDataCb()". Similarly, the read message can be seen in "ReadLocalDataCb"