Skip to main content
NKall.7
Associate II
Feb 26, 2019 4:38 AM UTC
Question

Which files do we need from the shared sample code for BNRG Mesh, so that we can create a custom smartphone application?

I am trying to create a custom Android app taking the reference of BNRG Mesh shared sample code. I am not able to create and start the network keeping smartphone as a provisioner. I am using Android plugin version 3.2.1 and Gradle version 4.6. Please help.

This topic has been closed for replies.

2 replies

alok
Visitor II
Feb 26, 2019 9:59 AM UTC

Hi NIshant,

Since you were able to compile the code and run the App earlier, you can change the images, text and App layout etc to make another App.

If you are using another approach, Kindly refer to the reference example to follow the similar scheme and APIs in the New App design

udidq
Associate II
Feb 27, 2019 5:09 AM UTC

Hello,

Also you can remove everything and keep only defaultAppCallback and mainactivity . Start with the sample project and keep only these two files.Sequence will be create network, start network => start getting callbacks for unprovisioned devices , use provision api to provision the node and then setRemote data to send command to it.

you can take help from the api guide to know how to use models and vendor commands

tx