Skip to main content
rdscliff
Associate III
Apr 21, 2019 11:22 PM UTC
Question

Where is the Project directory in the BlueNRG1-DK_3.1?

I want to rebuild the DTM application to run with a 16 MHz crystal. The DTM project used to be included in the 3.0 DK but it is not in the 3.1 DK. How do I get the project code?

    This topic has been closed for replies.

    2 replies

    Winfred LU
    ST Employee
    Apr 22, 2019 2:11 AM UTC

    Hi rdscliff,

    It will be under C:\Users\<ID>\ST\BlueNRG-1_2 DK 3.1.0\Project

    to avoid the issue of Windows Account control that normal users cannot access system folders like "Program Files".

    This has been described in the Release notes:

    • Library, Project, Utilities folders are located under {User} –> ST in order to be able to directly compile projects even with Windows User Account Control activated.

    Best Regards,

    Winfred

    rdscliff
    rdscliffAuthor
    Associate III
    Apr 22, 2019 3:54 AM UTC

    Thank you. I missed the line in the release notes. I found the files after searching my entire hard drive for the .c files. The <ID> turned out to be the administrator account.