Skip to main content
Padmashree_NS
Associate
Dec 3, 2020 9:24 AM UTC
Question

When OTA and bonding both features are enabled, the bond information gets erased from flash each time I disconnect from the device. Any suggestions on this?

I am using BLE Chat application where I have added the bonding feature. When I don't use OTA, I can connect to the device and bond it and the bond information stays even after reconnecting to the device.

But when the OTA is enabled, once I connect to the device and bond it and disconnect it the bond information is getting erased and the device is again asking to bond on reconnection.

    This topic has been closed for replies.