Skip to main content
markb
Associate III
Jul 27, 2015 2:23 PM UTC
Question

What settings are needed for client to resolve miniAP host name

Posted on July 27, 2015 at 16:23

Hi,

When the SPWF01 is in miniAP mode what setup will allow the client to resolve the module's domain name. Do I need to set ip_dns to be the module's IP address ?

Thanks,

Mark
    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Jul 27, 2015 3:13 PM UTC
    Posted on July 27, 2015 at 17:13

    Hi Mark,

    variable called ''ip_use_dhcp'' enables miniAP to run both dhcp and dns server feature. Clients (up to 5) can ask for ''ip_apdomainname'' resource, and miniAP can resolve that address to IP address.

    j