Skip to main content
PGonz.2
Visitor II
Jan 26, 2023 12:04 PM UTC
Question

What is the limitation of EVALKITSTKNX?? I can change the code to do other apliations, for example adding more Keys or LEDs? I can export this project to other STM32 microcontrollers to do my own board?

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Jan 26, 2023 12:42 PM UTC

    Welcome, @Pablo González Ortega​, to the community!

    The EVALKITSTKNX is initially only an evaluation platform with a given demonstration stack and binary from Tapko. A few LEDs or switches can be added via the source code (e.g. in evalkit_stknx.c, part of STSW-KITSTKNX).

    However, the library is only available as a pre-compiled binary, so for larger changes, such as changing the MCU platform or to your own board, you should contact its manufacturer TAPKO and license their stack (if you cannot do this yourself).

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.