Skip to main content
markb
Associate III
Jul 1, 2015 8:00 AM UTC
Question

What does +WIND:54:Dot11 AuthIllegal 0/2 signify?

Posted on July 01, 2015 at 10:00

Hi, I am getting the above error indication when trying to access an AP, what does it mean?

Cheers,

Mark

    This topic has been closed for replies.

    27 replies

    markb
    markbAuthor
    Associate III
    Jul 1, 2015 8:01 AM UTC
    Posted on July 01, 2015 at 10:01

    Sorry, the indication number in the title should be 45 not 54!

    Gerardo GALLUCCI
    ST Employee
    Jul 1, 2015 11:55 AM UTC
    Posted on July 01, 2015 at 13:55

    Hi Mark,

    WIND:45 means there was an error on authentication process.

    Check shared/open authentication setting between AP and STA.

    j

    markb
    markbAuthor
    Associate III
    Jul 1, 2015 12:13 PM UTC
    Posted on July 01, 2015 at 14:13

    Thanks for that but now I have a bigger problem in that I used stm32flash to load SPWF01S-150410-c2e37a3-RELEASE-main.bin and although I can read

    that back from the flash and it compares OK, the module no longer wants to talk to the MCU. Any idea what could have gone wrong?

    markb
    markbAuthor
    Associate III
    Jul 1, 2015 1:03 PM UTC
    Posted on July 01, 2015 at 15:03

    OK, I am very stupid. What I have managed to do is overwrite the loader at the bottom of flash memory with the new firmware because I didn't realise that it needs to be written at a higher address. So now I need to replace the code that goes at the bottom of flash but that doesn't appear to be available as a download. I have submitted a support request but who knows how long that will take. Could someone please read out the low part of flash memory into a hex file and attach it to this thread?

    Cheers,

    Mark

    Gerardo GALLUCCI
    ST Employee
    Jul 2, 2015 8:12 AM UTC
    Posted on July 02, 2015 at 10:12

    You can ask for it directly to your local ST support. Faster.

    markb
    markbAuthor
    Associate III
    Jul 2, 2015 9:05 AM UTC
    Posted on July 02, 2015 at 11:05

    Hi, thanks for the reply. ST support faster? Well, I submitted a support request yesterday and so far just got an automated response. I'm sure it would be faster if someone could just read out the low flash into a hex file and post it to the forum.

    Cheers,

    Mark

    Gerardo GALLUCCI
    ST Employee
    Jul 2, 2015 12:36 PM UTC
    Posted on July 02, 2015 at 14:36

    Hi Mark,

    I don't see support request in the system...

    Which link did you use?

    markb
    markbAuthor
    Associate III
    Jul 2, 2015 1:59 PM UTC
    Posted on July 02, 2015 at 15:59

    Sorry, I don't know which link I used. It was on the my.st.com website. The ticket I got was

    TECH008051

    .

    I wish someone would just read the first 0x2800 bytes out of the MCU flash and post the hex to this forum.

    Gerardo GALLUCCI
    ST Employee
    Jul 3, 2015 7:20 AM UTC
    Posted on July 03, 2015 at 09:20

    Ticket in on. You should get a reply very soon.

    Thanks for patience

    j

    markb
    markbAuthor
    Associate III
    Jul 3, 2015 9:12 AM UTC
    Posted on July 03, 2015 at 11:12

    OK, thanks but I gave up waiting and managed to read the flash from another module so my test module is up and running again. But I still have the original problem which is when it tries to associate with an AP it fails with:

    +WIND:45:Dot11 AuthIllegal 0/2

    +WIND:75:Rejected Association (0xD)

    I am using WPA/WPA2 and the text key is getting crunched. The AP is a TP-LINK TL-WA701N and works with all other WIFI devices I have.

    Could you give any more info about what is wrong here?

    Thanks