Skip to main content
dimitrybulkin
Associate II
Jul 7, 2014 7:45 PM UTC
Question

WF update. Socket speed

Posted on July 07, 2014 at 21:45

Hi,

1. I am using SOCKETS to make big file upload from my device from server. I have 2 questions:

a) What is maximum buffer size in module for SOCKET? It seems about 1K. After it makes unstable in operation

b) What is maximum speed of upload using sockets? I am acheaving 5-10 Kb/sec. It is too slow for me.

I send 800 bytes in socket. Wait for OK. Then send next part. Sometimes I see  delays/timeouts about 1.5s while awaiting ''OK'' from module. Or there is no OK at all. What's reason?

FW  version = 140128-caf4b79-SPWF01S

2. I am single developer (not a company). My distributor ignored me. Can you push them to send me fresh FW? Compel, Saint-Petersburg, Russia. My mail dimitrybulkin@yandex.ru

#wi-fi
    This topic has been closed for replies.

    17 replies

    dimitrybulkin
    Associate II
    Jul 13, 2014 7:05 PM UTC
    Posted on July 13, 2014 at 21:05

    Ciao, Gerardo

    Thanks for Phyton script. But result of using is the same to my experience with embeded.

    When I send small file ~2 kb to my server all is OK. When I send big file 500 kB I see that module go into some kind of fault and reset. Using embeded I can see some codes with info where fault happens. With Phyton I just see reset +WIND messages, no codes. 

    It is possible to avoid fails if I send trough embeded with this algorythm:

    Open socket

    Open file

    In cycle{

    Read file into buffer. Buffer must be not bigger than 450 bytes

    Send buffer with socket

    Wait for OK response

    }

    But after sending about 2-10 kB speed reduces. Because OK responce will can be after 0,8...1.5 seconds. So problem is not in boudrate of UART/

    I am very interesred to send big files to my server. So now I will devide big files into 2KB blocks, but it is bad solution. Help me to understand problem. Or if it is problem of module I am ready to help you solve it with my colaboration. I am realy like your module comparing Digi, microchip and TI solutions.

    I am ready to give you:

    1. access to my web server for tests

    2. files I am sending 

    3. my sources an explain them

    But not in forum because in files info how to acces to my server.

    dimitrybulkin
    Associate II
    Jul 13, 2014 7:10 PM UTC
    Posted on July 13, 2014 at 21:10

    2 kb file sending with phyton. File contains POST heads to get answer from my web server

    C:\PROJECT\SPWF01S_shell>SPWF01S_shell.py

    +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

                  SPWF01S Embedded Wifi Shell - SPG Application

      This PYTHON SOFTWARE was tested on Windows XP, Windows 7 and Linux Fedora

                     Python ver. 2.7.3, pyserial 2.5 package

    +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

    Insert the ComPort (i.e. COM4 or /dev/ttyUSB0) which is connected the SPWF01S mo

    dule: com3

    Insert the UART Baudrate of the module (i.e. 115200, 921600, ..): 230400

    HW Flow Control used <O for disabled, 1 for enabled>: 0

    The following serial port is opened: com3

     SPWF01S is connected to the PC

    ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

    +++++++++++++

     The available commands are:

     help -> shows the available shell commands

     network install -> saves OPEN, WEP, WPA/WPA2 config parameters and performs the

     connection

     miniap install -> saves MiniAP config parameters and starts the MiniAP

     mode -> sets the module operating mode (IDLE, STA, MINI AP)

     reset -> resets the module

     factory -> restores the factory default values of the config variables and rebo

    ots the module

     scan -> scans available Wifi networks

     readconf -> reads current module configuration parameters

     readvar -> reads a module parameter (see User Manual for the whole list)

     setvar -> saves a module parameter in NV memory and reboots

     readstat -> reads current module statistics

     peers -> returns the list and the statistics of devices connected to the module

     fwupdate -> performs an over-the-air firmware update

     fsupdate -> performs an over-the-air filesystem update (ext flash memory)

     fserase -> erases the content of the external flash memory

     webserver -> disable/enable the module's web server

     fsl -> lists the files stored in the module web server

     create file -> creates a file in the RAM memory and appends blocks of data

     fsp -> prints the contents of an existing file stored in the module web server

     fsd -> deletes an existing file (static files may not be deleted)

     ping -> sends a ping packet to the specified host

     httpget -> performs a single HTTP GET request to the named host and path

     httppost -> performs a post of the given path to the specified host

     radio -> enables/disables the wifi radio

     gpio control -> allows to configure, read or write a GPIO

     sockopen -> opens up to 8 TCP/UDP socket

     sockwrite -> allows to write data to socket

     sockquery -> returns the number of bytes of data waiting on socket

     sockread -> allows to read data from socket

     sockclose -> allows to close the socket

     powersave -> allows to enable the Power Save Mode

     sleep -> enables the Sleep Mode

     standby -> enables the Standby Mode

     active -> enables the Active Mode

     exit -> closes the application

    ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

    +++++++++++++

    Enter your commands below.

    Insert ''exit'' to leave the application.

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockopen

    Insert the target host: [HIDDEN]

    Insert the TCP/UDP port: 80

    Insert the socket type <t for TCP | u for UDP>: t

     ID: 00

    OK

    ++++++++++++++++++++++++++++++++++++++++++++++

     If you see something like this:

      ID: 00

     means that the socket 00 is correctly opened

    ++++++++++++++++++++++++++++++++++++++++++++++

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockwrite

    Insert the file source <console|localfile>: localfile

    Insert the socket identifier <from 00 to 07>: 00

    Insert the filename (the file must be located in the same shell folder): small.d

    at

    OK

    +WIND:55:Pending Data:0:390

    The data have been sent to the Socket Server

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockread

    Insert the socket identifier <from 00 to 07>: 00

    Choose an action <all=read all|len=bytes to read>: all

    HTTP/1.1 200 OK

    Server: nginx/1.6.0

    Date: Sun, 13 Jul 2014 18:35:32 GMT

    Content-Type: text/html

    Content-Length: 217

    Connection: keep-alive

    X-Powered-By: PHP/5.3.28

    <FILENAME>forsend.dat</FILENAME>

    <FILETYPE>text/plain</FILETYPE>

    <UPLOADERROR>0</UPLOADERROR>

    <TEMPRARYNAME>/var/tmp/php8ak0d6</TEMPRARYNAME>

    <LENGTH>1558</LENGTH>

    OK

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockclose

    Insert the socket identifier <from 00 to 07>: 00

    +WIND:58:Socket Closed:0

    ERROR: Illegal Socket ID

    Insert the name of the command (help=display the whole list, exit=close the APP)

    :

    So my server answered:

    <FILENAME>forsend.dat</FILENAME>

    <FILETYPE>text/plain</FILETYPE>

    <UPLOADERROR>0</UPLOADERROR>

    <TEMPRARYNAME>/var/tmp/php8ak0d6</TEMPRARYNAME>

    <LENGTH>1558</LENGTH>

    All is ok. File is recieved without problems.

    dimitrybulkin
    Associate II
    Jul 13, 2014 7:11 PM UTC
    Posted on July 13, 2014 at 21:11

    Now I send 500 kb file

    +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

                  SPWF01S Embedded Wifi Shell - SPG Application

      This PYTHON SOFTWARE was tested on Windows XP, Windows 7 and Linux Fedora

                     Python ver. 2.7.3, pyserial 2.5 package

    +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

    Insert the ComPort (i.e. COM4 or /dev/ttyUSB0) which is connected the SPWF01S mo

    dule: COM3

    Insert the UART Baudrate of the module (i.e. 115200, 921600, ..): 230400

    HW Flow Control used <O for disabled, 1 for enabled>: 0

    The following serial port is opened: COM3

     SPWF01S is connected to the PC

    ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

    +++++++++++++

     The available commands are:

     help -> shows the available shell commands

     network install -> saves OPEN, WEP, WPA/WPA2 config parameters and performs the

     connection

     miniap install -> saves MiniAP config parameters and starts the MiniAP

     mode -> sets the module operating mode (IDLE, STA, MINI AP)

     reset -> resets the module

     factory -> restores the factory default values of the config variables and rebo

    ots the module

     scan -> scans available Wifi networks

     readconf -> reads current module configuration parameters

     readvar -> reads a module parameter (see User Manual for the whole list)

     setvar -> saves a module parameter in NV memory and reboots

     readstat -> reads current module statistics

     peers -> returns the list and the statistics of devices connected to the module

     fwupdate -> performs an over-the-air firmware update

     fsupdate -> performs an over-the-air filesystem update (ext flash memory)

     fserase -> erases the content of the external flash memory

     webserver -> disable/enable the module's web server

     fsl -> lists the files stored in the module web server

     create file -> creates a file in the RAM memory and appends blocks of data

     fsp -> prints the contents of an existing file stored in the module web server

     fsd -> deletes an existing file (static files may not be deleted)

     ping -> sends a ping packet to the specified host

     httpget -> performs a single HTTP GET request to the named host and path

     httppost -> performs a post of the given path to the specified host

     radio -> enables/disables the wifi radio

     gpio control -> allows to configure, read or write a GPIO

     sockopen -> opens up to 8 TCP/UDP socket

     sockwrite -> allows to write data to socket

     sockquery -> returns the number of bytes of data waiting on socket

     sockread -> allows to read data from socket

     sockclose -> allows to close the socket

     powersave -> allows to enable the Power Save Mode

     sleep -> enables the Sleep Mode

     standby -> enables the Standby Mode

     active -> enables the Active Mode

     exit -> closes the application

    ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

    +++++++++++++

    Enter your commands below.

    Insert ''exit'' to leave the application.

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockopen

    Insert the target host: [HIDDEN]

    Insert the TCP/UDP port: 80

    Insert the socket type <t for TCP | u for UDP>: t

     ID: 00

    OK

    ++++++++++++++++++++++++++++++++++++++++++++++

     If you see something like this:

      ID: 00

     means that the socket 00 is correctly opened

    ++++++++++++++++++++++++++++++++++++++++++++++

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockwrite

    Insert the file source <console|localfile>: localfile

    Insert the socket identifier <from 00 to 07>: 00

    Insert the filename (the file must be located in the same shell folder): big.dat

    OK

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Command not found

    ERROR: Comma

    The data have been sent to the Socket Server

    Insert the name of the command (help=display the whole list, exit=close the APP)

    : sockclose

    Insert the socket identifier <from 00 to 07>: 00

    ERROR: Illegal Socket ID

    +WIND:32:WiFi Hardware Started

    +WIND:21:WiFi Scanning

    +WIND:35:WiFi Scan Complete (0x0)

    +WIND:19:WiFi Join:E0:2

    Insert the name of the command (help=display the whole list, exit=close the APP)

    :

    dimitrybulkin
    Associate II
    Jul 13, 2014 7:31 PM UTC
    Posted on July 13, 2014 at 21:31

    Module was connected to usbe trough http://www.terraelectronica.ru/pdf/CHIP45/LITTLEUSB.pdf

    Power is taken from DISCOVERY STM32F4 with 407 controller connected to USB trough miniusb (debuger)

    I have only suspection that DISCOVERY can't give enough power to send 500 kb file. Will make big capacitor in power circut and report you. But wifi module do not report that there is not enough power.

    So now if I send ~500 kb file with buffer 460 bytes

    I have low speed because of big delays to recieve OK from module. And mostly sending is OK

    And if I use 2048 bytes buffer I see... same. But few hours ago there are was messages about reboot! I made power off/on for module physicaly. Maybe that is reason. And remark: 2048 buffer is not faster than 460 bytes buffer. 

    Firmware is 140512-complete - FW3.0

    Gerardo GALLUCCI
    ST Employee
    Jul 15, 2014 9:54 AM UTC
    Posted on July 15, 2014 at 11:54

    Hi,

    now that setup is ok, you can use ST team for support: rf-support-emea@st.com

    thanks

    j

    dimitrybulkin
    Associate II
    Jul 16, 2014 2:57 AM UTC
    Posted on July 16, 2014 at 04:57

    Sorry

    What do you mean whan write ''

    now that setup is ok,

    ''?

    Gerardo GALLUCCI
    ST Employee
    Jul 16, 2014 8:52 AM UTC
    Posted on July 16, 2014 at 10:52

    You had right FW from Compel, and Python scripts too, so, you can now start evaluating SPWF01S features.

    ST RF team offers technical support on WiFi module and related tools.

    ciao

    j