Skip to main content
toby
Associate II
Jun 15, 2015 10:34 AM UTC
Question

WEP in AP mode

Posted on June 15, 2015 at 12:34

Is there a limitation/restriction of of the WEP key lengths in AP mode?

Set password to 'test1':

AT+S.SCFG=wifi_wep_keys[0],7465737431

AT+S.SCFG=wifi_wep_key_lens,05

This works OK.  I can connect fine with WEP authentication.

However trying :

Set password to 'test11':

AT+S.SCFG=wifi_wep_keys[0],746573743131

AT+S.SCFG=wifi_wep_key_lens,06

Doesn't work I can't connet to the access point?

However, if I change key to 14 bytes, and wep ley length to '0D' it seems to works again?

Can the length only be '05' or '0D'?

Thanks in advance.  (P.S. I am running 3.4 firmware).

    This topic has been closed for replies.

    2 replies

    toby
    tobyAuthor
    Associate II
    Jun 15, 2015 11:25 AM UTC
    Posted on June 15, 2015 at 13:25

    Just an update:

    Looking into this the WEP keys can only be 5 ASCII or 13 ASCII in length..

    So the 05 length works - However for a 13 ASCII key, the wifi_wep_key_lens needs to be set to 0D for some reason(14)!

    Seems to work then..

    Gerardo GALLUCCI
    ST Employee
    Jun 15, 2015 2:01 PM UTC
    Posted on June 15, 2015 at 16:01

    Hi Toby,

    Correct. wifi_wep_key_lens possible values are 05 and 0D

    ________________

    Attachments :

    WEP_key_config.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Hv&d=%2Fa%2F0X0000000bmi%2FSgXsQdCu6NIwrSNakVGtuzcqQr1tgUPHwByXhe8GKUY&asPdf=false