Skip to main content
NDvas.2
Associate
Dec 9, 2020 5:18 AM UTC
Question

We are developing a product that needs to support (and be powered from) either a PD power supply or a non PD power supply - we do not know which the user will connect. Can someone please let me know what is the right architecture here? Thank you, Ni

..

    This topic has been closed for replies.

    4 replies

    NDvas.2
    NDvas.2Author
    Associate
    Dec 9, 2020 10:07 AM UTC

    Sorry I forgot to mention we wish to use the STUSB4500

    Winfred LU
    ST Employee
    Dec 11, 2020 2:54 AM UTC

    Please refer to STEVAL-ISC005V1

    https://www.st.com/content/st_com/en/products/evaluation-tools/solution-evaluation-tools/psu-and-converter-solution-eval-boards/steval-isc005v1.html

    STUSB4500 is a standalone USB PD controller. When connecting to a Type-C supply, it recognizes that the supply does not have PD capability, then automatically consume the power with Type-C only (5V 3A ex).

    NDvas.2
    NDvas.2Author
    Associate
    Dec 14, 2020 8:34 AM UTC

    Thank you @Winfred LU​ 

    Two related questions for you, referring to the below paste from the STUSB4500 eval board schematics:

    1. You are saying that even when a non PD power supply is connected, the 4500 will assert the VBUS_EN_SNK pin low and by that enable power to travel from the VBUS to the VSNK output?
    2. Why are there two FETS (T1 + T4) here? Isn't one enough?

    Thank you again,

    Nir.

    0693W000006FbbSQAS.jpg 

    Winfred LU
    ST Employee
    Dec 17, 2020 6:31 AM UTC
    1. Yes, with an exception that if POWER_ONLY_ABOVE_5V is set (to high), the VBUS_EN_SNK pin is only asserted when either PDO2 or PDO3 (both are PD only) contract is established.
    2. T1 acts as an on/off switch ; T4 is to ensure Type-C receptacle is a cold socket - not turned on until something is plugged in

    If removing T1, it will not compliant with the standard. Therefore, it is not recommended to remove T1.

    If removing T4, there will be no negative voltage protection and no reverse battery protection. Thus, you may trade off keeping it against removing it based on your application needs.