Skip to main content
Visitor II
Apr 17, 2026 5:20 AM UTC
Solved

W6X_Init hangs on STM32F767VIT6 — sem_if_ready never posted despite DMA completing

I am porting the ST67W611M1 WiFi/BLE driver (X-CUBE-ST67W61 v1.2.0) from a NUCLEO-U575ZI-Q to a custom PCB with STM32F767VIT6. The Nucleo version works perfectly. On the F767 custom board, W6X_Init() hangs indefinitely.

HARDWARE
- Host MCU: STM32F767VIT6 (216MHz, Cortex-M7)
- WiFi module: ST67W611M1 (NCP firmware: mission_t01_v2.0.97.bin — confirmed flashed and verified)
- SPI2: PB12=NSS(SW), PB13=SCK, PB14=MISO, PB15=MOSI
- CHIP_EN: PD4, SPI_RDY: PD7 (EXTI rising+falling, NVIC enabled)
- DMA1 Stream3 (RX, CH0), Stream4 (TX, CH0)
- FreeRTOS heap: 102400, configMAX_PRIORITIES: 56
- LOW_POWER_MODE: disabled, W6X_CLOCK_MODE: 1 (internal RC)

SYMPTOMS
PuTTY output stops at:
W6X_Init...
[hangs forever]

W6X_Init() never returns. The FreeRTOS task blocks on sem_if_ready permanently.

DEBUG FINDINGS
I added debug prints to spi_port_transfer_dma() to log RX buffer contents. Here is what the module sends during init:

RX[0]=0D [1]=0A [2]=72 len=12 → "\r\nr..." (boot message start)
RX[0]=AA [1]=55 [2]=00 len=12 → SPI header
RX[0]=2B [1]=43 [2]=57 len=16 → "+CW..."
RX[0]=2B [1]=47 [2]=45 len=16 → "+GE..."
RX[0]=41 [1]=54 [2]=20 len=256 → "AT ..." (AT command exchange)
RX[0]=2B [1]=56 [2]=42 len=12 → "+VB..." (version/boot info)
RX[0]=2B [1]=45 [2]=46 len=12 → "+EF..." (EFUSE reads begin, loop forever)

The module IS responding. DMA completes every transaction (HAL_SPI_TxRxCpltCallback fires). The driver progresses through GetModuleInfo (reads GMR, VBAT, EFUSE) but sem_if_ready is never posted and W6X_Init never returns.

WHAT I HAVE TRIED
- Verified EXTI9_5 NVIC enabled for PD7
- DMA IRQ handlers present and calling HAL_DMA_IRQHandler
- Tried blocking SPI (HAL_SPI_TransmitReceive) — same hang
- Tried DMA (HAL_SPI_TransmitReceive_DMA) — DMA completes but still hangs
- Disabled D-Cache and I-Cache (SCB_DisableDCache/SCB_DisableICache) — no change
- configMAX_PRIORITIES=56 (above SPI engine task priority of 53)
- Removed all UART debug prints from ISR/callback context
- W6X_POWER_SAVE_AUTO=0, W6X_CLOCK_MODE=1
- NCP firmware reflashed and verified via NCP_get_chip_info.bat — chip info reads successfully

QUESTION
What is different about the STM32F767 that would prevent sem_if_ready from being posted? The SPI data exchange appears correct — the module is sending valid responses. Is there a known issue with the modem command handler parser on Cortex-M7, or a specific spi_port.c adaptation required for F767?

Any guidance appreciated. Happy to provide more debug output or code snippets.

Thank you.

Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Apr 28, 2026 4:33 PM UTC

Hello @carlosjoelcaceres ,

Could you please give us more information about the software you are using, the version, the SPI configuration (the maximum recommended frequency is 40MHz).

Also attached you will find an example project done for STM32F746. Please compare with your project to try to find any difference in the configuration of the SPI, for example, that could lead to this issue.

If you are still facing this issue, please feel free to provide your project for us to analyze it, because the host should not hang forever.


Hope this will help !
Regards
Louis

1 reply

Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Apr 28, 2026 4:33 PM UTC

Hello @carlosjoelcaceres ,

Could you please give us more information about the software you are using, the version, the SPI configuration (the maximum recommended frequency is 40MHz).

Also attached you will find an example project done for STM32F746. Please compare with your project to try to find any difference in the configuration of the SPI, for example, that could lead to this issue.

If you are still facing this issue, please feel free to provide your project for us to analyze it, because the host should not hang forever.


Hope this will help !
Regards
Louis