Skip to main content
MDoc.1
Associate
Oct 8, 2021 3:14 AM UTC
Question

w

..

    This topic has been closed for replies.

    3 replies

    LCord.1
    Associate II
    Oct 8, 2021 9:10 AM UTC

    Same I even get "WrMulti failed to send 32768 bytes to regsiter 0x00" (32768 is 0x8000 why would you send 32kibyte?) when I use get_set_params sketch.

    I get "Beginning transmission to 14; Writing 1 bytes to register 0x7FFF

    Write Status: 2

    " twice and then "VL53L5CX not detected at requested address" if I use ranging_basic sketch. Hope somebody can beak it down. Thanks in advance

    Edit: I use the ESP32 and maybe that is the cause I'll be using an arduino to test it. 

    AMehr.3
    Visitor II
    Nov 4, 2021 1:11 AM UTC

    Any update on this?

    Did the Arduino work?

    MDoc.1
    MDoc.1Author
    Associate
    Oct 8, 2021 9:32 AM UTC

    In my case, I didn't get any error except that if i dont disable the _vl53l5cx_poll_for_answer() function, the system freezes due to the do while loop inside the function, the device does not respond. I guess it has something to do with my WrMulti function.