Skip to main content
RAdam.1
Associate III
Apr 17, 2020 2:53 PM UTC
Solved

Using double precision in a DMA callback seems to block it?

I am using a BlueNRG-LP and started with the CCA01M1 I2S project. I changed the callback so that it applies a volume to the stream in real time. But this seems to block the code if I use a double (which id like to do to see some precision - and I want to add a tone generator in there too). If I use a int16_t then it is fine and doesnt block,

If variable c is double then it blocks. If c is int then it works

anyone know why?

 /*Copy song fragment to Audio Output buffer*/

for(i=0; i< DMA_BUFFER_SIZE/2; i++)

{  

if (Amplifier.State == AMP_PLAYING)

{

c = *Amplifier.PlayPtr;

c /= 10;

c *= Amplifier.Volume;

d = (int16_t) c;

Amplifier.DMABuffer[i*2]= d; 

Amplifier.DMABuffer[i*2+1]= d; 

Amplifier.PlayPtr++;

} 

    This topic has been closed for replies.
    berendi
    berendiBest answer
    Principal
    Apr 17, 2020 3:08 PM UTC

    It has a CPU with no hardware floating point operations, all floating point calculations are computed by a software library. It takes a lot of time.

    Use integer multiplications and bit shifts only.

    4 replies

    berendi
    berendiBest answer
    Principal
    Apr 17, 2020 3:08 PM UTC

    It has a CPU with no hardware floating point operations, all floating point calculations are computed by a software library. It takes a lot of time.

    Use integer multiplications and bit shifts only.

    RAdam.1
    RAdam.1Author
    Associate III
    Apr 17, 2020 3:18 PM UTC

    Thanks berendi... your response is probably correct. Although simply changing the order of the math seems to make it work or not.

    c = Fragment1[song_position];

    mult = vol/10;

    c *= (double) mult;

    works ok. But ...

    c = Fragment1[song_position];

    c /= 10;

    c *= (double) vol;

    blocks it...

    As you say maybe it is just the way the optimizer works or something to make it faster or slower.

    Shame I cant create a tone or sweep on the fly (it uses the sin function) - I'll need to create it offline and just have it copied in from Flash which is a waste of storage

    berendi
    Principal
    Apr 17, 2020 3:36 PM UTC

    mult = vol/10; is a constant expression that the optimizer can move outside the loop, so it has to be calculated only once. In the original code, the division is performed on the sample in every loop iteration, so there are only half as many floating operations to calculate.

    Using float instead of double should be even faster. You don't need double precision if the result is converted to 16 bits.

    RAdam.1
    RAdam.1Author
    Associate III
    Apr 17, 2020 3:52 PM UTC

    That makes absolute sense! Thanks so much for your kind help and clarity!