Skip to main content
philippe1
Associate III
Feb 3, 2015 7:49 AM UTC
Question

updated UM1755 doc?

Posted on February 03, 2015 at 08:49

Hi everyone, 

I was wondering if there is an updated version for the UM1755 which (partially) describes the commands available for the BlueNRG chipset. I can't find decoding scheme for the VS HCI events for example.

Thank you.
This topic has been closed for replies.

11 replies

marchese.graziella
Visitor II
Jan 15, 2016 11:40 AM UTC
Posted on January 15, 2016 at 12:40

Dear Customer,

here below the description:

0x04- Event type

0xff - HCI_VENDOR;

0x3-Parameter Total Length;

0x01,0x00 - (0x0001 little endian) - Evt_Blue_Initialized

01 - Reason_Code ->Firmware started properly

This event occurs when the BlueNRG-MS firmware is started normally, it gives a Evt_Blue_Initialized event to

the user to indicate the system has started (with Reason Code 0x01).

Regards,

GM

Could you please help me with this frame ?

Thank you.

04 ff 03 01 00 01