Skip to main content
mhemetsberger9
Associate
Aug 10, 2015 8:55 AM UTC
Question

Unable to initiate TLS Connection using SPWF01SA.11 wit FW V3.4

Posted on August 10, 2015 at 10:55

Dear Community,

I have generated RSA signed certificates using OpenSSL as described in application note AN4683.

I also started a server using openssl command and the generated certificates as described on page 20 of AN4683.

Then I used:

AT+S.TLSCERT2=clean,all

->resppnse of WIFI module: OK

AT+S.SETTIME=<seconds>

->resppnse of WIFI module: OK

AT+S.TLSCERT=f_ca,<size><CR><data>

->resppnse of WIFI module: OK

AT+S.TLSDOMAIN=f_domain,<server domain>

->resppnse of WIFI module: OK

AT+S.SOCKON=<host-ip>,<port>,s,ind

->response of WIFI module: ERROR: Unable to load CA certificate

Does anybody know what am I doing wrong? Thanks for you help, regards Michael!

#tls-spwf01sa.11
    This topic has been closed for replies.

    11 replies

    Nickname3786_O
    Visitor II
    Aug 14, 2015 9:12 AM UTC
    Posted on August 14, 2015 at 11:12

    Hi Michael,

    you can add the parameter ''-tls1_2'' to the openssl server in order to force the TLS 1.2 security on the server side.

    In this case, the module has to connect to the server using the TLS instead of SSL 3.0.

    Regards,

    Salvo