Skip to main content
DMill.10
Visitor II
Nov 23, 2021 8:48 PM UTC
Question

Unable to debug or program steval-IDB008V1M using ST-LinkV3.

https://community.st.com/s/question/0D53W00000TFnQJSA1/unable-to-debug-or-program-stevalidb008v1m-using-stlinkv2

The question in the link above is exactly similar to mine, but instead I am using a ST-LinkV3 debugger instead of their V2. I figured I would ask this question again since no one has answer in a long time.

I am using WISE-Studio and when I try and run an example project this is the console output with it being unsuccessful:

Open On-Chip Debugger 0.11.0+dev-00062-g6405d35f3-dirty (2021-03-26-11:44)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : auto-selecting first available session transport "dapdirect_swd". To override use 'transport select <transport>'.

Info : STLINK V3J8M3B5S1 (API v3) VID:PID 0483:374F

Info : Target voltage: 3.287759

Info : Unable to match requested speed 1200 kHz, using 1000 kHz

Info : Unable to match requested speed 1200 kHz, using 1000 kHz

Info : clock speed 1000 kHz

Info : stlink_dap_op_connect(connect)

Info : SWD DPIDR 0x0bb11477

Info : bluenrg-2.cpu: hardware has 4 breakpoints, 2 watchpoints

Info : starting gdb server for bluenrg-2.cpu on 3333

Info : Listening on port 3333 for gdb connections

Error: Fail reading CTRL/STAT register. Force reconnect

Info : stlink_dap_op_connect(reconnect)

Info : SWD DPIDR 0x0bb11477

Info : AP write error, reset will not halt

Error: timed out while waiting for target halted

** Unable to reset target **

shutdown command invoked

Warn : Flash driver of bluenrg-2.flash does not support free_driver_priv()

But, if I try and run the same program from the blueNRG-2 Navigator, I have no issue going through the direct usb connection. If someone could help out with this that would be amazing.

Thanks!

    This topic has been closed for replies.

    1 reply

    Laurent LOUAZON
    ST Employee
    Dec 1, 2021 10:21 AM UTC

    Hello,

    I guess the problem is related to the fact debugging interface is disabled when BluenRG-2 (or BlueNRG-M2 module) is using an FW with sleep mode enabled.

    Please have a look at DT0120 design tip available on st.com.

    When using Navigator tool, you will not face problem as this tool will handle DIO7 (bootloader pin) of BlueNRG-2/BlueNRG-M2 from STM32L1 present on eval kit.

    It will force BlueNRG-2 DIO7 to "1" before doing a reset so that BlueNRG-2 will remain in bootloader.

    When trying to flash from any IDEs, you must force DIO7 to "1" before doing a HW reset or a power on / power off.

    If willing to debug any application with SWD interface, and as said in in DT0120, , you should have disable sleep mode in your application or add a delay before entering sleep mode.

    Regards

    Laurent