Skip to main content
armando
Associate
Mar 31, 2015 11:45 PM UTC
Question

Unable to connect to TCP Socket (server) using SPWF01S

Posted on April 01, 2015 at 01:45

Hi all, 

I really hope somebody can help me on this. I'm using a STEVAL-IDW001v1 with SPWF01S module integrated. I'm trying to connect to a local server using TCP socket, right now I'm using the server socket.exe example from the wifi training hands on doc(page). Use this command:

''at+s.sockon=192.168.69.79,32000,t''

and I get this error

''ERROR: Failed to connect''

any idea?

here my dump keys:

♯ Dumping All Configuration Keys:

 

♯  nv_manuf = ST

 

♯  nv_model = SPWF01SA1

 

♯  nv_serial = 4313D12184

 

♯  nv_wifi_macaddr = 00:80:E1:FF:DC:D7

 

♯  blink_led = 1

 

♯  user_desc = anonymous

 

♯  localecho1 = 1

 

♯  console_uart = 1

 

♯  console1_speed = 115200

 

♯  console1_hwfc = 0

 

♯  console1_enabled = 1

 

♯  console2_speed = 115200

 

♯  console2_enabled = 0

 

♯  localecho2 = 1

 

♯  console3_enabled = 0

 

♯  console3_speed = 115200

 

♯  localecho3 = 1

 

♯  wifi_tx_msdu_lifetime = 0

 

♯  wifi_rx_msdu_lifetime = 0

 

♯  wifi_rts_threshold = 3000

 

♯  wifi_ssid = 43:6F:6C:69:62:72:69:41:70:70:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

♯  wifi_ssid_len = 10

 

♯  wifi_mode = 1

 

♯  wifi_auth_type = 0

 

♯  wifi_rssi_thresh = 0

 

♯  wifi_rssi_hyst = 0

 

♯  wifi_ap_idle_timeout = 120

 

♯  wifi_beacon_loss_thresh = 10

 

♯  wifi_priv_mode = 2

 

♯  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

♯  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

♯  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

♯  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

 

♯  wifi_wep_key_lens = 00:00:00:00

 

♯  wifi_wep_default_key = 0

 

♯  wifi_wpa_psk_raw = C3:87:6B:99:19:8D:B7:AB:6A:3A:B7:B8:46:9F:CF:4E:20:66:07:AA:69:89:7C:65:96:DC:62:83:7C:2D:92:A5

 

♯  wifi_wpa_psk_text = chupala11veces

 

♯  ip_use_dhcp = 1

 

♯  ip_use_httpd = 1

 

♯  ip_mtu = 1500

 

♯  ip_hostname = iwm-FF-DC-D7

 

♯  ip_apdomainname = captiveportal.net

 

♯  ip_ipaddr = 192.168.0.50

 

♯  ip_netmask = 255.255.255.0

 

♯  ip_gw = 192.168.0.1

 

♯  ip_dns = 192.168.0.1

 

♯  ip_http_get_recv_timeout = 1000

 

♯  ip_dhcp_timeout = 20

 

here my statistics:

 

♯ Status & Statistics:

 

♯  version = 140225-02d76c4-SPWF01S

 

♯  reset_reason = 2

 

♯  conf_flag = 5

 

♯  system_uptime = 4393

 

♯  system_sleeptime = 0

 

♯  gpio_enable = 0

 

♯  captiveportal = 0

 

♯  wifi_sup_ratemask = 0x003FFFCF

 

♯  wifi_bas_rate_mask = 0x0000000F

 

♯  wifi_state = 10

 

♯  wifi_dtim_period = 1

 

♯  wifi_gf_mode = 0

 

♯  wifi_channelnum = 6

 

♯  wifi_chan_activity2 = 0x00000FFE

 

♯  wifi_max_tx_power = 18

 

♯  wifi_reg_country = MX

 

♯  wifi_num_assoc = 0

 

♯  ip_ipaddr = 192.168.69.79

 

♯  ip_netmask = 255.255.255.0

 

♯  ip_gw = 192.168.69.1

 

♯  ip_dns = 192.168.52.1

 

♯  free_heap = 25104

 

♯  min_heap = 23584

 

♯  current_time = 10202

attached is the document where I'm working as a reference.

looking forward to hear from somebody :)

#spwf01s-wifi #socket-server
    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    Apr 1, 2015 10:21 AM UTC
    Posted on April 01, 2015 at 12:21

    Hi,

    I see, from ip_ipaddr status variable, that module's IP address (the one contained into WIND:24 after association) that module IP is 192.168.69.79

     

    Are you opening a socket from module to module itself?