Question
TSC1641 dynamic addresses for more than 4 devices
Im developing a custom board with a non ST microcontroller, the board has 6 mosfets and i wish to monitor them using ST's TSC1641
Is it possible to have 6 of the aforementioned sensors to monitor each mosfet? Also is the exposed pad at the center really to be left isolated or can it be connected to ground?
If its possible to use the 6 devices in i3c how would the adress assignment look like? how would the devices know the assignment was to them?
Ive left a0 and a1 connected to a 3 way solder bridge so i can place a shunt to power or ground in each