Welcome @TomLH, to the community!
Well, the TS555 was developed decades ago and the specifications found in the data sheet were set at that time. The 0.4…1.5V only applies to 25°C, at other temperatures it must be ensured that RESET can be triggered correctly, i.e. the voltage must drop to a level of ≤0.3V to trigger.
On the other hand, it must also be taken into account that RESET may only be triggered from 2.0V.
Typically, a temperature other than 25°C will be present, so the full temperature range specification applies so that STMicroelectronics can guarantee the parameters under all circumstances.
Hope that answers your question?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.