Skip to main content
Visitor II
Sep 21, 2026 6:03 AM UTC
Solved

Timing parameters for ULPI interface DDR Mode - STULPI01BTBR

Hi,

 

In the STULPI01BTBR datasheet I could find the timing spec only for SDR mode. I need to verify the DDR mode on our board and could not find the DDR mode timing spec. Can anyone please help to find the timing spec for ULPI interface DDR Mode.

 

Regards,
Shivakumar

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 21, 2026 6:52 AM UTC

Welcome ​@Spuran, to the community!

ULPI DDR uses 4-bit data clocking, is an optional feature of the ULPI Specification 1.1, and is not implemented in the STULPI01B.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Sep 21, 2026 6:52 AM UTC

Welcome ​@Spuran, to the community!

ULPI DDR uses 4-bit data clocking, is an optional feature of the ULPI Specification 1.1, and is not implemented in the STULPI01B.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.