Skip to main content
Wpian
Associate
May 21, 2019 7:31 AM UTC
Question

the last two parameter of aci_gap_set_discoverable(......,SlaveConnIntervMin,SlaveConnIntervMax)

according to the BlueNRG-MS Bluetooth LE stack aci :aci_gap_set_discoverable(......,SlaveConnIntervMin,SlaveConnIntervMax) 

the last two parameter value range :0x0006~0x0c80,

but the STM32CubeExpansion_BLE1_V4.40

why the last two parameter are 0???

l

    This topic has been closed for replies.

    2 replies

    Winfred LU
    ST Employee
    May 22, 2019 3:31 AM UTC

    Giving 0 for parameters Slave_Conn_Interval_Min or Slave_Conn_Interval_Max means :

    not to specify minimum or maximum Slave Connection Interval.

    Wpian
    WpianAuthor
    Associate
    Jun 21, 2019 9:18 AM UTC

    Dear Winfred,

    thanks for your answer.

    not to specify minimum or maximum Slave Connection Interval means the Slave Connection Interval can be random? Besides, I don‘t understand the relationship between ADV_interval and Slave_Conn_interval ,would you please make an explain?Thanks.