Skip to main content
TSane.1
Associate
Jul 7, 2020 8:28 PM UTC
Question

The aci_gap_pairing_complete_event is not called for random passkey response on version V1.0.0 ?

 Which stack release do I need to pull this in, I am currently using V1.0.0.

The issue I see, seems similar, where in I don't see the paring complete ever being called (rarely called or not returned at all).

My Initiator parameters are (BLE112D)

Io capability 7 (Display with Keyboard), mitm enabled, encryption key min size 7, bonding enabled.

The peripheral is a bluenrg, with authentication details.

ret = aci_gap_set_authentication_requirement(  BONDING,

                              MITM_PROTECTION_REQUIRED,

                              SC_IS_SUPPORTED,    

                              KEYPRESS_IS_NOT_SUPPORTED,

                              7,

                              16,

                              DONOT_USE_FIXED_PIN_FOR_PAIRING,

                              pincode,

                              PUBLIC_ADDR);

Are these requirements for authentication valid ?

And does this seem a relatable issue to ID 5284?

This topic has been closed for replies.