Skip to main content
ESuwa.1
Visitor II
May 24, 2021 10:35 PM UTC
Question

TESEO LIV3F - update rate says 10Hz, does that mean it is updating location based on satellite data at 10Hz? Or is it using interpolated data ? Does this module have an integrated IMU?

..

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    May 24, 2021 10:43 PM UTC

    Tracking GNSS signals is a continuous process, the tracking here in a consumer receiver is likely to be in the 50/60 Hz range. The solution rate from the measurements tends to be slower as it is more computationally intensive, rather than tracking the velocity/acceleration of the satellites vs receiver.

    The solution tends to be stale, where the time of measurements is provided, you should understand time/motion in your own implementation, and extrapolate.

    >>Does this module have an integrated IMU?

    Reading the marketing bullet-points one would assume not.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..