Associate III
Sep 2, 2026 5:13 AM UTC
Solved
TCPP03-M20 not powering up USB-C port
- 5 replies
- 68 views
Hi, i am using the TCPP03-M20 for the first time. This device is stand alone. i have the device setup for 5V, which is all that is required. there is no power to the device initially when connected to the USB-C port. CC1c and CC2c pins are at around 1.65V. i do not see any voltage on Vbus. have attached the schematic section for this circuit. .If i apply 3.3v to Vcc_Vconn VBUS is still 0V. Any help appreciated.
Mark