Skip to main content
Visitor II
May 28, 2025 12:30 PM UTC
Question

Sub1GHz module

Hi,

 

I would like to explore the possibility of using the sub1GHz product solution from ST, particularly, the part number S2-LPTX.

Here are the requirements

1. We need One Receiver and 4 Transmitter (as shown in the image) which are operating at 433MHz ISM bands.

2. Need to send data from all 4 transmitters to the one receiver simultaneously

Q1: Is it possible to pair 4 no's transmitters to the receiver by the help of the MCU on board?

Q2. Is there any co-existence issue occur when we operate more than one unit if it is placed close by (1 Unit = 4 Tx +     1Rx) 

Q3. If simultaneous data transmission mentioned in point 2 not possible, will time multiplexed mode of operation possible?

Q4. Do we need to implement any SW based protocol to avoid co-existence issues?

Q5. Is there any particular procedure to take care during pairing of Tx and Rx?

Q6. What could be the possible coverage distance if we use these modules?

 

 

AshnoJames_0-1748435550932.png

 

This topic has been closed for replies.