Skip to main content
Dwang.3
Associate
Mar 8, 2021 4:02 PM UTC
Solved

STUSB4710A not found

Hi everyone, I am new for STUSB4710A. I connect STUSB4710a STEVAL_ISC004v1 evaluation board to my laptop, through a min b usb cable. when I run the graphic interface en.stsw-stusb001, there is one error: usb error: no target found. please connect first the evaluation board with a usb cable. I powered on / off the device. The software still does not find the STUSB4710A. shall install some drivers? Thanks.

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Mar 9, 2021 2:47 PM UTC

    Let's make a little clearer about what you need to do:

    • for 1.1 step 1 (Connect) ... step 8 (Drag and drop) you only need the NUCLEO board and a Mini USB cable, which gets unplugged in step 10; during these steps the STEVAL-ISV004V1 must not yet be connected
    • after that, for 1.1 step 11 you don't need the Mini USB cable anymore, but now the NUCLEO + STEVAL-ISV004V1 + Micro USB cable

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    7 replies

    Peter BENSCH
    ST Technical Moderator
    Mar 8, 2021 4:13 PM UTC

    Did you read the UM2254 (STSW-STUSB001 quick installation guide)?

    The introduction says:

    In order to run the GUI on a laptop, an STM32 Nucleo board must be programmed to act as a USB to I²C bridge between the laptop and the STUSB evaluation boards.

    Good luck!

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Dwang.3
    Dwang.3Author
    Associate
    Mar 8, 2021 4:22 PM UTC
    Hi ST,
    Thanks a lot for the prompt answer. Yes, I read the manual. And I see step 2
    [cid:image001.jpg@01D7143F.903952D0]
    But when I connect STUSB4710A, I did not see the driver installation.
    So at step 8, I can not see STM32 Nucleo drive.
    [cid:image002.jpg@01D7143F.903952D0]
    Do you know why? Thanks.
    BR
    Da ****
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Mar 9, 2021 2:47 PM UTC

    Let's make a little clearer about what you need to do:

    • for 1.1 step 1 (Connect) ... step 8 (Drag and drop) you only need the NUCLEO board and a Mini USB cable, which gets unplugged in step 10; during these steps the STEVAL-ISV004V1 must not yet be connected
    • after that, for 1.1 step 11 you don't need the Mini USB cable anymore, but now the NUCLEO + STEVAL-ISV004V1 + Micro USB cable

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Dwang.3
    Dwang.3Author
    Associate
    Mar 10, 2021 10:43 AM UTC

    Hi Peter,

    Thank you so much. Indeed, I was wondering it should have not been so complex. Yes, I misunderstood something. Thanks again.

    Gregory Go.
    Senior III
    Mar 17, 2021 10:26 PM UTC

    Hello,

    There may be some confusion because the STUSB4710 GUI v3.2.3 requires 2 USB cables:

    - one USB-mini cable (connected to STM32 Nucleo board)

    - one USB-micro cable (connected to STUSB4700 eval board)

    This can make the setup complicated.

    An alternative is to use the GUI v3.5 which only needs 1 USB-mini cable (connected to STM32 Nucleo board).

    You can download it here:

    https://community.st.com/s/question/0D53W00000HySKa/stusb4700-gui-offline

    Associate
    Apr 14, 2025 8:17 PM UTC

    Thanks for you assistance! Four years later and you have resolved my issue. I responded on my thread showing your response as I am sure it will help other members. FYI... GUI v3.5 is not even on the ST website, they are still showing the v3.2.