Question
STUSB4700 USB-C Power sourcing on a Slave device
- 0 replies
- 582 views
Hi,
I'm beginner in USB-C and USB_PD some things are not clear for me.
We developing a device which is a USB SLAVE Device - not HOST (Virtual comport device - datalogging to a notebook)
This device has a large battery, so we want to charge the notebook from this device.
We want to keep things simple and use the STUSB4700 to enable up to 100W charging power.
Can the device supply charge power and still work as USB slave device?
Can the attached circuit work?
Regards
Falko
PS Forum Software:
> The following labels are not available here: USB-PD
Why can't i use label "USB-PD" ? Othe people was using it?