Skip to main content
Associate II
May 9, 2025 5:28 AM UTC
Solved

STUSB1600

Hello,

I have questions about the STUSB1600:

1. Mouser marks the device as "obsolete". What is the EOL of the STUSB1600 and what alternative is recommended (STUSB1700?)?

2. The STUSB1600 is connected to the MP1 via I2C. I need to program the NVM "in system" with custom values but did not find / missed the information (in the datasheet) on how to do so. Any Idea (apart from the external programming with this NUCLEO board)?

 

This topic has been closed for replies.
EOFBest answer
Associate II
May 23, 2025 6:33 AM UTC

Thank you for the feedback.

I was hoping to make the configuration persistent by issuing some commands via I2C from the MP1 to the STUSB1600 like for example "0x42: Writes the content of the configuration into NVM".

I guess this possibility does not exist.

10 replies

RobK1
Associate II
May 9, 2025 6:42 AM UTC
EOFAuthor
Associate II
May 9, 2025 6:56 AM UTC

Yes, exactly. I Wonder why Mouser sets it to obsolete....

EOF_0-1746773666469.png

 

EOFAuthor
Associate II
May 9, 2025 6:58 AM UTC

Ah I see: The STUSB1600QTR is "obsolete" but the "STUSB1600AQTR" is not!

Thank you for the clarification!

NBALL
ST Employee
May 23, 2025 6:19 AM UTC

Hello

1- STUSB1600AQTR is the valid reference (stusb1600qtr has been replaced by this one since long time). This is the reference used on MP1 board.

2- To program STUSB1600 in system, stsw-stusb004 can be used as example.

Best regards

Nathalie

EOFAuthorBest answer
Associate II
May 23, 2025 6:33 AM UTC

Thank you for the feedback.

I was hoping to make the configuration persistent by issuing some commands via I2C from the MP1 to the STUSB1600 like for example "0x42: Writes the content of the configuration into NVM".

I guess this possibility does not exist.

NBALL
ST Employee
May 23, 2025 7:24 AM UTC

There is flow to follow to write the NVM: it is not possible to access unitary bit: it needs to be access by 'bank'

Unitary bit can be access thru I2C only

EOFAuthor
Associate II
May 23, 2025 8:16 AM UTC

How does the "bank" writing work? Is there a (protocol) description somewhere?