Skip to main content
Associate
Apr 30, 2024 2:30 PM UTC
Solved

STPM33/34 MISO & Insulating barrier

Hello everyone

I am looking into the STPM33/34. I only want to use 1 SPI bus for both ICs and select it with the SCS.

In the datasheet I cannot see whether the MISO goes into tristate when the IC in question is not active.

I also cannot see any information about the galvanic isolation/barrier.

Can anyone give me information about this.
Thank you in advance.

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
May 17, 2024 7:23 AM UTC

Hi,

>I also cannot see any information about the galvanic isolation/barrier.

Right, because there is no isolation/barrier .

If you feel a post has answered your question, please click on " Best Answer ".

12 replies

Didier HERROUIN
ST Technical Moderator
Jun 14, 2024 9:04 AM UTC

Hello,

The MISO line is in Hi-Z mode when the STPM3x is not selected (SCS at high level).

Just note this limitation in case you use several STPM3x in parallel: 
https://www.st.com/resource/en/errata_sheet/es0591-stpm3x-device-limitations--stmicroelectronics.pdf

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.