Skip to main content
Associate III
Nov 12, 2022 9:00 AM UTC
Solved

STM32U5 - OSPI - GPDMA. Driving an AMOLED display (GRAM) with QSPI - blocking mode working but not with GPMDA.

Hi, I am Driving an AMOLED display (GRAM) with QSPI.

In blocking mode everythings works fine, but now I trying to "update" it using GPDMA, nothing works. Any advices ?

So in blocking mode I used the typical :

OSPI_RegularCmdTypeDef sCommand = {0};
	 sCommand.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
 
	 sCommand.Instruction = 0x02;
	 sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
	 sCommand.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
 
	 sCommand.Address = address<<8;
	 sCommand.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
	 sCommand.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
 
 
 
	 sCommand.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
 
	 sCommand.DataMode = HAL_OSPI_DATA_1_LINE;
	 sCommand.NbData = nbOfData;
	 sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
	 sCommand.SIOOMode = HAL_OSPI_SIOO_INST_ONLY_FIRST_CMD;
 
	 sCommand.DummyCycles = 0;
 
HAL_OSPI_Command(&hospi1, &sCommand, 1000);
HAL_OSPI_Transmit(&hospi1, param, 1000);

Which works perfectly,

Now in the DMA, i replaced the HAL_OSPI_TRANSMIT with :

HAL_OSPI_Transmit_DMA(&hospi1, param);

I also updated the CubeMX configuration :

0693W00000WIAlVQAX.pngand for GPDMA:

0693W00000WIAnCQAX.pngTo be honnest at a certain point I tried all the possibilities with GPDMA port - direction - and so on with no success, so I kept what made more sens to me.

Can someone point me out my mistakes or a way to dig into ?

Thanks for your time and your help.

Regards

This topic has been closed for replies.
BerthaBest answer
Associate III
Apr 16, 2023 9:44 AM UTC

Ok, I dig more into it, I figured out that if datasent count is lower that 0xFFFF then HAL_OSPI_Transmit_DMA works as expected. But in the case of sending more data it "breaks".

I made a bug report and waiting ST response on that, here with minimal code to reproduce:

https://community.st.com/s/question/0D53W00002DWC4xSAH/halospitransmitdma-not-working-for-nbdata-0xffff-

3 replies

Tesla DeLorean
Guru
Nov 12, 2022 2:26 PM UTC

Not sure.

Watch for caching and coherency issues.

Make sure memory is within reach of the DMA unit.

Watch for errors/status indicators about why a particular transfer failed.

QPSI part not identified.

Shift of address by eight suggests you're not handling it properly, if you need dummy cycles use those, don't shift the address. Mask the address so it fits within the scope of the QSPI part.

DMA is going to need more handling/management code.

You showed code that works, not the code that doesn't. Present the code that doesn't work, with ALL the associated handlers and callbacks.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BerthaAuthorBest answer
Associate III
Apr 16, 2023 9:44 AM UTC

Ok, I dig more into it, I figured out that if datasent count is lower that 0xFFFF then HAL_OSPI_Transmit_DMA works as expected. But in the case of sending more data it "breaks".

I made a bug report and waiting ST response on that, here with minimal code to reproduce:

https://community.st.com/s/question/0D53W00002DWC4xSAH/halospitransmitdma-not-working-for-nbdata-0xffff-

Associate II
Apr 5, 2025 5:25 PM UTC

Hi Bertha. I’m currently working on driving an AMOLED display using the STM32U5. Could I kindly ask how you initialize the OCTOSPI or share any relevant experience? I’m writing an OCTOSPI driver to read the IC ID of the AMOLED display driver, but it keeps returning 0x00000000. I have the code and datasheet on my personal homepage. If you have time, could you please help me? I’d be most grateful!
https://community.st.com/t5/stm32-mcus-products/stm32u585-octospi-not-reading-device-id-from-icna3306-amoled/m-p/790473