Skip to main content
Oshrit Elma
Visitor II
Sep 27, 2017 1:57 PM UTC
Question

STM32L476JEY BootLoader after FOTA

Posted on September 27, 2017 at 15:57

In my program i'm doing FOTA via BLE.

I developed my code with Nucleo-l476RG EVB and Nucleo-IDB05A1,

 based on the 

FP-SNS-FLIGHT1 program.

Now I'm working with my custom PCB using STM32L476JEY as MCU and 

BlueNRG-MS and have problem with system reset.

I can see all the packets 

transferred successfully with correct CRC. I write the firmware to address 0x08040008 and add the magic number to 0x08040000. Then, when resetting with HAL_NVIC_SystemReset() function the old program is restarted.

The __ICFEDIT_intvec_start__  address was: 0x08000000, so I supposed that my program takes the bootloader place and Ichanged it to 0x08004000, also the VECT_TAB_OFFSET to 0x4000.

0690X00000608HAQAY.png

With these changes  the reset doesn't work in any case, even before doing OTA via BLE. I can just flash my program from IAR.

I'll be happy with any ideas ,

thanks

#fota #stm32l476 #bluenrg #system-reset
This topic has been closed for replies.