Skip to main content
kasi viswanadh
Associate II
Apr 27, 2021 12:51 PM UTC
Solved

stm32l476, will Different SPI busses interfere each other if one of the the SPI peripheral stops working?

I'm using stm32l476jgy6 MCU, it has 3 SPI busses, I'm using all of 3 SPI busses for different peripherals. If peripheral on SPI1 fails to communicate with MCU, will it cause any effect on other SPI busses? I've a scenario where I'm using BLUENRG-MS on SPI1, lsm6dsm and lsm303agr sensors on SPI2, external SPI flash on SPI3. all of these peripherals are not working, but when lsm303agr removed from the board, rest of the components started communicating to MCU. there is no code blockage, controller is running continuously. I'm using Sensor tile as a base hardware design, ALLMEMS as a base firmware.

Need help understanding the issue

Thanks

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Apr 27, 2021 8:20 PM UTC

"If peripheral on SPI1 fails to communicate with MCU, will it cause any effect on other SPI busses?"

Not as such.

But, if your software locks-up - that will cause problems!

Also, if the peripheral failure has other hardware implications - such as overloading power supplies - that could also cause problems.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

2 replies

Andrew Neil
Andrew NeilBest answer
Super User
Apr 27, 2021 8:20 PM UTC

"If peripheral on SPI1 fails to communicate with MCU, will it cause any effect on other SPI busses?"

Not as such.

But, if your software locks-up - that will cause problems!

Also, if the peripheral failure has other hardware implications - such as overloading power supplies - that could also cause problems.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
kasi viswanadh
Associate II
Apr 29, 2021 8:03 AM UTC

Thank you very much Andrew Neil for the reply.