Skip to main content
sai
Associate II
Nov 11, 2015 10:44 AM UTC
Question

STM32L053 half duplex mode

Posted on November 11, 2015 at 11:44

Hello,

I am using STM32L053R6 interfaced to Blue NRG chip. I am accessing the blue NRG through VCOM.

I have connected a USB to UART converter to a PC and was trasmitting the VCOM data over this. It worked!!!

Now, I want to do the same in half duplex mode. I have designed a circuit for the USB to UART converter so that it acts as a single wire UART. It seems to work as I can see the data being sent to STM32.

But however, there is no response from the controller. I doubt even if it is reading this data.

Can you please check if my half duplex configuartion is right?

  GPIO_InitTypeDef  GPIO_InitStruct;

 

  /*♯♯-1- Enable peripherals and GPIO Clocks ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

  /* Enable GPIO TX/RX clock */

  USARTx_TX_GPIO_CLK_ENABLE();

  USARTx_RX_GPIO_CLK_ENABLE();

  /* Enable USART1 clock */

  USARTx_CLK_ENABLE();

 

  /*♯♯-2- Configure peripheral GPIO ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ 

  /* UART TX GPIO pin configuration  */

  GPIO_InitStruct.Pin       = USARTx_TX_PIN;

 GPIO_InitStruct.Mode      = GPIO_MODE_AF_OD;

  GPIO_InitStruct.Pull      = GPIO_PULLUP;

  GPIO_InitStruct.Speed     = GPIO_SPEED_FAST;

  GPIO_InitStruct.Alternate = USARTx_TX_AF;

 

  HAL_GPIO_Init(USARTx_TX_GPIO_PORT, &GPIO_InitStruct);

  

  GPIO_InitStruct.Pin = USARTx_RX_PIN;

  GPIO_InitStruct.Alternate = USARTx_RX_AF;

   

  HAL_GPIO_Init(USARTx_RX_GPIO_PORT, &GPIO_InitStruct);

And then,

  UartHandle.Instance        = USARTx;

 

  UartHandle.Init.BaudRate   = 9600;

  UartHandle.Init.WordLength = UART_WORDLENGTH_8B;

  UartHandle.Init.StopBits   = UART_STOPBITS_1;

  UartHandle.Init.Parity     = UART_PARITY_NONE;

  UartHandle.Init.HwFlowCtl  = UART_HWCONTROL_NONE;

  UartHandle.Init.Mode       = UART_MODE_TX_RX;

 

 if(HAL_UART_Init(&UartHandle) != HAL_OK)

  {

    // Initialization Error

    Error_Handler();

  }

 if(HAL_HalfDuplex_Init(&UartHandle) != HAL_OK)

 {

     Error_Handler();

 }

#nucleo #half-duplex-usart #bluenrg
This topic has been closed for replies.