Skip to main content
jp1
Associate II
Mar 14, 2016 6:48 AM UTC
Question

STM32 BLE ToolBox App

Posted on March 14, 2016 at 07:48

We're using the STM32Nucleo + BlueNRg Expansion HRM profile with Android smartphone as a master.  The connection interval is ~ 50 ms as dictated my the master.

We would like to get access to the Android app''STM32 BLE ToolBox'' source code.

The intent is to adjust the connection interval from the default 50 ms to 1 to 2 seconds.

Is it possible to get a link where we can download the source code from?

Any other suggestions to increase the connection interval are welcome.

Thanks,

-JP

#ble-connection-interval
This topic has been closed for replies.

2 replies

Andrea Palmieri
ST Employee
Mar 17, 2016 12:26 PM UTC
Posted on March 17, 2016 at 13:26

Dear Customer,

The app source code is not currently publicly available.

Anyway, in order to change/update the connection parameters you should use the API “aci_l2cap_connection_parameter_update_request()� sent from the slave to the master once the connection is established.

Kind regards,

Andrea

We're using the STM32Nucleo + BlueNRg Expansion HRM profile with Android smartphone as a master.  The connection interval is ~ 50 ms as dictated my the master.

We would like to get access to the Android app''STM32 BLE ToolBox'' source code.

The intent is to adjust the connection interval from the default 50 ms to 1 to 2 seconds.

Is it possible to get a link where we can download the source code from?

Any other suggestions to increase the connection interval are welcome.

Thanks,

-JP

jp1
jp1Author
Associate II
Mar 28, 2016 7:34 AM UTC
Posted on March 28, 2016 at 09:34

Hi,

The code was commented out for 32L4.. Works after un-commenting ans setting the desired connection interval.

Thanks.

JP