Skip to main content
AlexandreR
Associate II
Jan 15, 2025 10:13 AM UTC
Solved

STKNX Linear regulator dropout

Hi,

I would like the DC/DC converter of STKNX to make 5V.

Also, I want the Linear regulator to make 3.3V

Because of global efficiency, I wanted to power the linear regulator with the 5V output of DC/DC converter.

I'm surprised that the datasheet specifies VDD_REGIN minimum voltage 6.8V, if VCC_SEL is shorted to ground (in order to make 3.3V linear regulator output).

Same for VDD_REGIN minimum voltage specified 8.5V, if VCC_SEL is shorted to VCC_Core (in order to make 5V linear regulator output).

This makes 3.5V voltage dropout, which seems pretty much to me.

 

Question: Is there a typography error in Datasheet? Or is the dropout of internal regulator as much as 3.5V ?

 

Many thanks,

   Alexandre

 

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 15, 2025 4:17 PM UTC

It is not a typo, but has to do with the fact that it is not an LDO, but a simple linear regulator whose dropout voltage can actually be that high. You will have noticed that VDD_REGIN for 5V is also at least 3.5V higher in table 5 one line below.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 15, 2025 4:17 PM UTC

It is not a typo, but has to do with the fact that it is not an LDO, but a simple linear regulator whose dropout voltage can actually be that high. You will have noticed that VDD_REGIN for 5V is also at least 3.5V higher in table 5 one line below.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AlexandreR
Associate II
Jan 15, 2025 4:27 PM UTC

Thank you Peter for this reply.

I have noticed it is 3.5V for both working modes.

I wish it was just an error, as it may have saved me space on a dense circuit. Also,I think requiring 5V and 3V3 is quite common.

BR,

   Alexandre