Skip to main content
SBart.5
Associate II
Jun 13, 2024 1:02 PM UTC
Question

STKNX: Is there a value for the maximum case temperature?

Hi,

during maximum heating tests of our device, we measured a case temperature of +92 °C on the STKNX (on top of the plastic package via thermocouple). The environmental temperature near the STKNX and the PCB was +85 °C.

On the borderline, but ok in my opinion.

To make things easier, is there perhaps a maximum value for the STKNX case temperature?

 

Datasheet information:

TJ =  Maximum operating junction temperature = +110 °C
TAMB = Operating ambient temperature = -40 to +85 °C

This topic has been closed for replies.