Skip to main content
idolezal
Associate II
Dec 14, 2022 9:47 AM UTC
Question

STEVAL-IDB008V1M (BlueNRG-2 SoC) does not establish VCP port on PC, only STM DFU

Since the poorly soldered microUSB connector on the eval board broke off, I fixed and wired USB-A connector. If the board is then connected to PC, STM DFU device appears in Device Manager and appropriate driver could be installed so I suppose that the wiring is O.K. However, originally a USB Serial Port (COMx) appeared so either the RF-Flasher Utility or a terminal program can work with the board.

What could be the cause of this?

This topic has been closed for replies.

1 reply

idolezal
idolezalAuthor
Associate II
Jan 3, 2023 3:53 PM UTC

What is the cause that the STM32L151 MCU (USB to UART converter) goes into the programming mode of itself (STM Device in DFU Mode)? Specific level on a pin? MCU had to be programmed before the eval board is launched but it can be done by MCU JTAG connector.