Skip to main content
EBono
Visitor II
May 6, 2019 7:50 AM UTC
Question

steval bluemic-1 read or write characteristics

Hi everyone,

I'm working with an steval bluemic-1 board and a nucleo with x-nucleo-idb05a1 expansion. For the moment i'm only able to notify a characteristic, but now i also want to read or write. bluemic-1 is the server, i want to receive the read request, update the characteristic and then allow the gatt to send the response. What i did since now is adding the characteristic as the following:

aci_gatt_add_char(service_handle,

              UUID_TYPE_128,

(Char_UUID_t *) my_UUID,

              8,

CHAR_PROP_READ,

ATTR_PERMISSION_NONE,

GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP,

16,

1,

              (uint16_t*)&AccHandle);

As you can see i use the "CHAR_PROP_READ" to set it as readable and "GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP" to be notified when a read occurs. Then i implement the "aci_gatt_read_permit_req_event" (that should be given to the application when a read request is received if i'm not wrong) in which i update my characteristic using the "aci_gatt_update_char_value" and then i allow the gatt to response using the "aci_gatt_allow_read". On the client, when i press the user button i send a read request using the "aci_gatt_read_charac_val". Debugging i see that on the client the read request starts correctly, but on the server side i didn't receive the "aci_gatt_read_permit_req_event". In a similar way if i add the characteristic using "CHAR_PROP_WRITE", sending an "aci_gatt_write_charac_descriptor" (from the client), i didn't receive the "aci_gatt_attribute_modified_event" on the server. I noticed that i receive that event only if i set the characteristic as "CHAR_PROP_NOTIFY".

What's wrong in my project? how can i read/write a characteristic?

Thanks

Enrico

    This topic has been closed for replies.