Skip to main content
KMiya.1
Associate
Oct 1, 2020 12:53 PM UTC
Question

STDC14 connector on BLUENRG-M2SA for VCP function of STLINK-V3SET

Hello everyone.

Can I make a STDC14 connector on BLUENRG-M2SA?

I want to use VCP function through STLINK-V3SET.

Do you have the following Pin assignment?

STDC14(Pin No.)_(Description)_>>>_BLUENRG-M2SA(Pin name)_(Pin No.)

STDC14_01___Reserved__________>>>___NC______________NC

STDC14_02___Reserved__________>>>___NC______________NC

STDC14_03___T_VCC_____________>>>___VDD (to Vin)____VDD

STDC14_04___T_JTMS/T_SWDIO____>>>___JTMS-SWTDIO_____Pin-13

STDC14_05___GND_______________>>>___GND_____________GND

STDC14_06___T_JCLK/T_SWCLK____>>>___JTCK-SWTCK______Pin_12

STDC14_07___GND_______________>>>___GND_____________GND

STDC14_08___T_JTDO/T_SWO______>>>___???_____________???

STDC14_09___T_JRCLK/NC________>>>___NC or BOOT ???__NC or Pin-07 ???

STDC14_10___T_JTDI/NC_________>>>___NC ???__________???

STDC14_11___GNDDetect_________>>>___GND_____________GND

STDC14_12___T_NRST____________>>>___RESETN__________Pin-19

STDC14_13___T_VCP_RX__________>>>___TXD_____________Pin-10

STDC14_14___T_VCP_TX__________>>>___SPI_CS1/RXD_____Pin-11

Thank you.

This topic has been closed for replies.